FLIR Wins Awards Worth Up to $23M from US Customs and Border Protection for Improved Ground and Air Surveillance Capabilities
Contracts Will Support CBP’s Mobile Surveillance Capability, and Low Altitude Autonomous Safety and Situational Awareness for Officers Programs
ARLINGTON, Va., January 13, 2021 ― FLIR Systems, Inc. (NASDAQ: FLIR) announced it has received awards from the United States (U.S.) Customs and Border Protection (CBP) to deliver improved air and ground surveillance capabilities using advanced thermal imaging and drone technology. All awards are potentially worth more than $23 million, including for delivery of the next-generation FLIR LVSS™ (Lightweight Vehicle Surveillance System) for CBP’s Mobile Surveillance Capability (MSC) program and delivery of FLIR SkyRaider™ drone tether kits, FLIR StormCaster™-T sensor payloads, and other technology for CBP’s Low Altitude Autonomous Safety and Situational Awareness for Officers (LASO) program. The LASO contract has a base value of $545,000 and was awarded from a competitive General Solicitation under authority of the Department of Homeland Security’s Commercial Solutions Opening Pilot Program.
The MSC order is for 19 new FLIR LVSS systems that will be deployed on the southwest and northern U.S. borders. Following delivery, CBP will have a total of 27 LVSS units deployed, fitted with TacFLIR® 380-HD cameras and FLIR R20SS radar. In November, the company delivered a capability upgrade to CBP’s current fleet of R80D SkyRaider UAS, including tether kits and StormCaster-T thermal payloads.
"Whether on the ground or in the air, FLIR world-class imaging and drone-based technologies give the men and women of U.S Customs and Border Protection nimble, rugged and reliable surveillance solutions for the toughest of environments,” said Roger Wells, VP and general manager of the Unmanned Systems and Integrated Solutions business at FLIR. “The expanded LVSS deployments and airborne sensor enhancements will deliver tangible benefits for these two programs. We’re proud of our longstanding partnership with CBP and honored that agents who serve on our nation’s borders are using FLIR technology to augment their efforts.”

The FLIR LVSS™ provides the most advanced, integrated surveillance available that can track up to 500 objects at once at ranges greater than 10 miles (16 km). LVSS is well suited to missions that call for speed, mobility and flexibility, including protecting remote borders, shorelines, and forward operating bases. A single operator can deploy and operate the system’s 16-foot mast from the cab of a pickup truck in less than 30 seconds.
The FLIR LVSS provides the most advanced, integrated surveillance available that can track up to 500 objects at once at ranges greater than 10 miles (16 km). LVSS is well suited to missions that call for speed, mobility and flexibility, including protecting remote borders, shorelines, and forward operating bases. A single operator can deploy and operate the system’s 16-foot mast from the cab of a pickup truck in less than 30 seconds. Payloads can be customized to each mission, with options for radar, thermal imagers, lasers, illuminators, weather station, or other intrusion sensors.
The FLIR SkyRaider tether kit is a modular, highly transportable system that will enhance CBP's existing SkyRaider fleet by providing persistent mission support. The tether can deliver power to aircraft and payloads for flights lasting up to 24 hours. The StormCaster-T features a FLIR Boson™ thermal camera for powerful object detection, recognition and identification day or night, with maximum range and time-on-station. Its continuous zoom lens enables long distance surveillance and reconnaissance while providing clear, actionable imagery.
For more about FLIR Systems’ border security solutions, visit www.flir.com/surveillance/border-surveillance/.
# # # #
About FLIR Systems, Inc.
Founded in 1978, FLIR Systems is a world-leading technology company focused on intelligent sensing solutions for defense and industrial applications. Our vision is to be “The World’s Sixth Sense,” creating and advancing technologies to help professionals make better, faster decisions that save lives and livelihoods. For more information, please visit www.flir.com and follow @flir.