New Software Update for Griffin G510

/contentassets/8427cd001844413a9e72584013c9b644/flir-griffin-g510-banner.jpg

Teledyne FLIR is pleased to announce a new software release for the Griffin G510 GC/MS (gas chromatograph mass spectrometer). This software update, 4.1.3.0 is available to all G510 customers.

 

This software update contains Turbo Fault Recovery, Saturation Detection, and various bug fixes.

 

Turbo Fault Recovery

A faulting turbo required a restart of the system prior to GSS 4.1.3.0.
Now, if a turbo faults (such as due to over heating) it will take the
system into a powered down state and present a diagnostic message.
The turbo fault will auto clear upon power up if possible.

 

Saturation Detection

Saturation detection has been added for the G510 and G510E.
Saturated areas of a result will be shown with a blue overlay on the
Chromatogram as well as a “SAT” message on any saturated targets.
This information will also be reflected in the GSSL1T reports.

 

Bug Fixes
  • Resolved a potential application lockup when running
    Conditioning methods.
  • Added a check on the Conditioning page to prevent a negative
    value from being set on the TIC.
  • Peaks were not scaled properly on extracted and library
    spectrum graphs in the GSSL1T result report when run in SIM
    mode.
  • Changed to Display Idle time now take effect without a
    software restart.


For information on updating your current Griffin G510 software, please contact our support team at Support for CBRNE Detection | Teledyne FLIR or [email protected].