identiFINDER R700 November Webinars [Completed]
This event has already completed.
Teledyne FLIR is pleased to announce the upcoming free virtual webinars for the new identiFINDER® R700. This webinar will include a mix of videos, demonstrations, and presentations.
The identiFINDER R700 is a highly sensitive backpack or fixed-location radiation detector.
This webinar will discuss:
- Connect up to and control up to four R700's through one Android or iOS device
- Use new built-in WiFi capabilities to network these devices
- Use greater coverage and directionality with multiple devices to reduce the time to locate and identify a radiological threat
This webinar will show case a check point scenario and demonstrate the steps to network up to four R700's on one Android or iOS device.
There are three webinars on November 20th, 2025, at 9:00 AM and 1:00 PM, and 9PM EST (UTC-05:00). Webinars are hosted on Microsoft Teams.
The webinars are approximately 1 hour long.
Sign-up is completely free.